CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / CimPointEnumField Json Schema
CimPointEnumField Json Schema
Description
Represents a point enum field that associates a text string with an integer point value.
Overview
CimPointEnumField
Represents a point enum field that associates a text string with an integer point value.
Text : string
The Text property gets and sets the text of the point enum field.
Value : integer
The numeric value of the point enum field.
SetpointAllowed : boolean
The SetpointAllowed property gets and sets if a setpoint is allowed with this enum text for the point.
Properties
NameDescriptionData Type
The Text property gets and sets the text of the point enum field.string
The numeric value of the point enum field.integer
The SetpointAllowed property gets and sets if a setpoint is allowed with this enum text for the point.boolean
See Also